Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24707
  • Release Date : 2019/02/27 09:00
  • Print

Connecting a USB interface of a personal computer to a programmable controller

The personal computer, with GX Works2 installed, only has a USB interface.
How can I connect the personal computer to a programmable controller?
Category : 

Answer

・ The FX-USB-AW can be used for the programmable controllers except for the FX3S/FX3G/FX3GC series.
・ Since the FX3S/FX3G/FX3GC series have the built-in USB port, a personal computer can be connected using a USB cable, GT09-C30USB-5P or MR-3JUSBCBL3M.

To use the FX-USB-AW, install the USB driver provided with the FX-USB-AW, on the personal computer.
For details on how to install the USB driver, refer to the following.
Appendix 16 in the GX Works2 Version 1 Operating Manual (Common) (Manual number: SH-080779ENG)

* The personal computer can also be connected to the FX3U and FX3UC series using the FX3U-USB-BD.
Product Name
FX-USB-AW, FX3U-USB-BD
Product Category
Main unit, Accessories, Options, Engineering Software, GX Works2, GX Developer
Series
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries