FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > High-Speed Counting > Operation error of the instruction that handles the present value of a high-speed counter
FAQ
Operation error of the instruction that handles the present value of a high-speed counter
The applied instruction that handles the present value of the high-speed counter cannot be executed due to an operation error.
Answer
The present value register of the high-speed counter is the 32-bit register. The applied instruction handling the 32-bit register must be the 32-bit instruction.
If the 16-bit instruction is used, an operation error occurs.
If the 16-bit instruction is used, an operation error occurs.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- High-Speed Counting
May I have your opinion?
Related FAQ
- Receiving short pulses
- MELSEC-F series high-speed counter blocks that can import differential pulses
- How to use built-in high-speed counters
- No communication between a programmable controller and a personal computer (GX Developer) after the communication parameters for the RS-232C communication equipment are set
- Repair term for the FX programmable controllers after discontinuation of production