Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24913
  • Release Date : 2019/04/17 11:39
  • Print

Differences in the specifications between the programmable controllers used in Japan and overseas.

What are the differences between the programmable controllers used in Japan and overseas?
Category : 

Answer

The input signal forms are different. All the programmable controllers for the domestic market other than the FX3G/FX3U series are the sink input. The programmable controllers for the overseas market and the FX3G/FX3U series can switch the sink/source input. Also, transistor outputs differ between the sink output type and source output type.
All the products of the FX3G/FX3U series are compliant with the overseas standards.
For the models other than the FX3G/FX3U series, the products for the overseas market are compliant with overseas standards.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries