FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Connecting special adapters to FX3U series
FAQ
Connecting special adapters to FX3U series
Are any interface modules required for connecting special adapters to FX3U series?
Answer
An expansion board is required. (However, it is not required when connecting only the special high-speed I/O adapter.)
- Product Name
- MELSEC-F Series
- Product Category
- FX3U
- Series
- Main Unit, I/O Extension
May I have your opinion?
Related FAQ
- Cable provided with the FX2N series extension unit
- 24+ terminal connection of an extension block
- Power supply cable of the input extension blocks for the connector type programmable controllers
- CF cards that can be used in the FX3U-CF-ADP
- Extension blocks and units that can be used in the FX3U series