FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Extension blocks and units that can be used in the FX3U series
FAQ
Extension blocks and units that can be used in the FX3U series
Is it possible to use the FX0N series extension blocks and units with the FX3U series?
Answer
The operation is not guaranteed. Please select the extension blocks and units from FX2N series.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U
- Series
- Main Unit, I/O Extension
May I have your opinion?
Related FAQ
- Connecting special adapters to FX3U series
- Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3UC series
- Cable provided with the FX2N series extension unit
- Number of files that can be created inside a CF card in the FX3U-CF-ADP
- 24+ terminal connection of an extension block