FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Positioning Control > Starting time of the FX3U-1PG
FAQ
Starting time of the FX3U-1PG
How long does it take to actually drive the FX3U-1PG after the operation command is turned on?
Answer
It takes 1 ms or less in a unit of the motor system and 2 ms or less in a unit of the machine system.
* Motor system∙∙∙The pulse number is used as the standard for the position command.
Machine system∙∙∙μm, mdeg, and 10-4 inch are used as the standard for the position command.
* Motor system∙∙∙The pulse number is used as the standard for the position command.
Machine system∙∙∙μm, mdeg, and 10-4 inch are used as the standard for the position command.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Output frequency of the FX3U-1PG pulse output block
- Terminal layout of the FX3U-1PG and FX2N-1PG pulse output blocks
- Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
- Positioning blocks/module that can be connected with a manual pulse generator
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block