FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Station number setting in the "PLC System(2)" tab of PLC Parameter setting on GX Developer when non-protocol communication is performed
FAQ
Station number setting in the "PLC System(2)" tab of PLC Parameter setting on GX Developer when non-protocol communication is performed
To perform the non-protocol communication with the FX programmable controller, how should I specify the station number setting in "PLC System(2)" of PLC parameter setting on GX Developer?
Answer
The station number setting is not required for non-protocol communication.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit, Network/Communication
May I have your opinion?
Related FAQ
- File format that can be saved to a CF card in the FX3U-CF-ADP
- Target address change during the positioning operation in the FX3U-1PG
- Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
- Number of GOTs (GOT1000 series) that can be connected to a FX3U-ENET-L
- Using the inverter communication instruction in FX3G series