Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24969
  • Release Date : 2019/04/23 07:19
  • Print

Connection of the FX3G series and the GT1020/GT1030 series (5 V type)

Is it possible to add the FX3G-422-BD to the FX3G series, and connect two GT1020/GT1030 series (5 V type) GOTs; one to the built-in port and the other to the extension port?
Category : 

Answer

Only one GT1020/GT1030 series (5 V type) can be connected to the FX3G series. To connect two GOTs, select the GT1020/GT1030 series (24 V type).
Product Name
MELSEC-F Series
Product Category
FX3G
Series
Main Unit

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries