Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 25221
  • Release Date : 2019/09/02 16:01
  • Print

Regarding failure of maximum resolution setting of MELIPC

I have connected a display that supports MELIPC's maximum resolution, but I cannot select the maximum resolution
in the "Display resolution" setting of Windows. What could be the cause?
Category : 

Answer

If you connect a display using a converter such as a display switch or DisplayPort-HDMI converter adapter,
you may not be able to select a high resolution. Refer the following points.
・ Connect the display directly to the MELIPC
・ Replace the converter
Product Name
MELIPC
Series
MI5000
MI2000
MI1000
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?