Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 25222
  • Release Date : 2019/09/02 16:01
  • Print

Regarding failure of communication with MI5122-VW via Ethernet

Communication failed with MI5122-VW via Ethernet, what shall I check?
Category : 

Answer

Check the IP address of the connected device for a duplicate IP address.
If your computer has multiple network connections, check that there are no devices with the same IP address
for network connections other than those to which the MI5122-VW is connected.
Product Name
MELIPC
Series
MI5000
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?