Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 38044
  • Release Date : 2021/02/25 17:54
  • Print

Checking the IP address of EcoWebServerIII

How to check the IP address of EcoWebServerIII?
Category : 

Answer

(1) Open the front cover on the server section, and set the MODE switch to the "STOP" position.
(2) Set the RESET switch to the "SEL." position.
(3) After the "CF CARD" LED turns off, turn the RESET switch to the "RES."
(4) After all the LEDs except the "POWER" LED on the power supply section turn off, return the RESET switch to the central position.
(5) Wait until the product starts up and the IP address is displayed on the 7-segment LED at the front.
Product Name
Energy Saving Data Collecting Servers
Series
EcoWebServerIII

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries