• No : 20804
  • Release Date : 2018/08/22 16:24
  • Print

FR-HAL/FR-HEL selection

When using the vector motor, should I select the FR-HAL/FR-HEL of the one-rank higher capacity for the vector motor?
Category : 

Answer

Not required. Select it according to the capacity of the vector motor used.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option