• No : 20954
  • Release Date : 2018/08/22 16:25
  • Print

FR-A8AL

When using the SF-V5RU and the 24 VDC power supply of the FR-A8AL for the encoder power supply, how should I wire them?
Category : 

Answer

When the PG24 terminal and the PG terminal are shorted, 24 VDC power for the encoder can be supplied from the PG24 terminal.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option