• No : 21081
  • Release Date : 2018/08/22 16:25
  • Print

FR-PU07

Can I connect the FR-PU07 to FR-A800/F800 directly?
Category : 

Answer

No. They can be connected with the connection cable (FR-CB20[]). [] indicates cable length (1 m, 3 m, 5 m).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800, option