• No : 21118
  • Release Date : 2018/08/22 16:26
  • Print

Copy function

Can parameters be copied to the A800/F800 series by using the copy function of the parameter unit (FR-PU07(BB))?
Category : 

Answer

No. (Using the copy function causes an error.) Use the FR-DU08 when performing the copy function of the operation panel.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800