- No : 21126
- Release Date : 2018/08/22 16:26
-
Print
Selection
Which is suitable for controlling the hydraulic pump, FR-A700 or FR-F700P?
- Category :
-
Answer
It is not completely recommended to use F700P because the starting torque at low speed of the hydraulic pump may be larger than that of the normal pump. Select the capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- Others