- No : 21143
- Release Date : 2018/08/22 16:26
-
Print
FR-RC
What is the setting values of Pr.30 and Pr.70 when the FR-RC is connected?
- Category :
-
Answer
Pr.30 = "1" and Pr.70 = "0".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ