• No : 21144
  • Release Date : 2018/08/22 16:26
  • Print

Wiring length

What is the total wiring length when an inverter and a terminal block are connected with a wire of 100m and a terminal block and five motors are connected with wires of 20m for example?
Category : 

Answer

The total wiring length is as follows: 100 m + (20 m × 5) = 200m.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ