- No : 21161
- Release Date : 2018/08/22 16:26
-
Print
Setting resolution switching
The display does not change even Pr.811 (Set resolution switchover) is set to "1". Are there any other parameters to be set?
- Category :
-
Answer
Check the setting value of Pr.37 (Speed display). When the machine speed is set, Pr.811 is disabled. Change the setting to the rotation speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700