- No : 21162
- Release Date : 2018/08/22 16:26
-
Print
Orientation control
After the X22 signal is turned ON, the motor keeps rotating at the speed of the setting value of Pr.351 (Orientation speed). What is the possible cause?
- Category :
-
Answer
The following reasons are possible.
- The signal of Z phase does not exist. (It is not returned normally.)
- The setting of Pr.359 encoder rotation direction is reversed.
- The setting of Pr.369 number of encoder pulses is not correct.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700