- No : 21168
- Release Date : 2018/08/22 16:26
-
Print
MD-CX522
The forward rotation is enabled, but reverse rotation is disabled. Is any setting required?
- Category :
-
Answer
The initial value of Pr.78 (Reverse rotation prevention selection) of the MD-CX522 is "1" (reverse rotation is disabled). When performing forward rotation and reverse rotation, set Pr.78 to "0". When performing only reverse rotation, set Pr.78 to "2".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Others