- No : 21175
- Release Date : 2018/08/22 16:26
-
Print
FR-SW1-SETUP
Is FR-SW1-SETUP compatible with the FR-S500?
- Category :
-
Answer
It is compatible with the -R type FR-S500. (It is not compatible with the FR-S500 without -R because it does not have the PU connector and thus cannot be connected with the personal computer.) The FR-S500E is compatible as well.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Others