- No : 21200
- Release Date : 2018/08/22 16:26
-
Print
Wiring length
Which capacity, inverter or motor, should be referred for the total wiring length between the inverter and motor?
- Category :
-
Answer
Refer to the inverter capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700