- No : 21230
- Release Date : 2018/08/22 16:26
-
Print
Checking bit state by CC-Link communication
Can I check the ON/OFF of the bit from CC-Link communication with monitor code: H0F (input terminal status)?
- Category :
-
Answer
Because the H0F monitor only observes the ON/OFF of the hardware, it cannot be checked.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700