- No : 21232
- Release Date : 2018/08/22 16:26
-
Print
Speed command by CC-Link communication
Can the speed command from CC-Link communication be compensated from the first terminal?
- Category :
-
Answer
It is not possible when the speed command is communication.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700