- No : 21233
- Release Date : 2018/08/22 16:26
-
Print
PID control of CC-Link communication
It is described that X14 signal is not necessary when performing the PID control with CC-Link communication (Pr.128 (PID action selection) = 50, 51, 60, 61). What happens when the X14 signal is assigned to the input terminal?
- Category :
-
Answer
When performing the PID control by CC-Link communication, the X14 signal is disabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700