- No : 21236
- Release Date : 2018/08/22 16:26
-
Print
Monitor code of CC-Link communication
When Pr.37 (Speed display) and Pr.144 (Speed setting switchover) are changed, does the monitor with the code: H01 (output frequency) switch to rotation speed or machine speed display?
- Category :
-
Answer
The monitor with the code H01 switches by changing Pr.37 and Pr.144.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700