- No : 21238
- Release Date : 2018/08/22 16:26
-
Print
Remote input signal of CC-Link communication
This is related to the remote input signal (RX1B (remote station ready)) sent from the inverter (FR-A7NC) to the master module. In the Instruction Manual of FR-A7NC, it is described that the signal becomes 0 when the inverter error occurs (protective function operation). If the RES signal turns ON, will the signal be 0?
- Category :
-
Answer
The signal becomes 0 when the RES signal is turned ON.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700