- No : 21241
- Release Date : 2018/08/22 16:26
-
Print
Pr.268 (Monitor decimal digits selection) during CC-Link communication
When Pr.268 (Monitor decimal digits selection) is changed, is the unit of data that is monitored by CC-Link communication changed?
- Category :
-
Answer
No, it is not changed. Pr.268 is the parameter for the operation panel.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700