• No : 21276
  • Release Date : 2018/08/22 16:26
  • Print

Noise filter

Is the noise filter built-in the FR-E700 series?
Category : 

Answer

The noise filter is not built-in the FR-E700 series.
It is built in the FR-A700/F700 series with the 55K or lower capacity.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700