• No : 21309
  • Release Date : 2018/08/22 16:26
  • Print

Model setting in FR-Configurator

With the FR-E740, when the automatic recognition is selected in the model setting of FR-Configurator (FR-SW3-SETUP-WJ), "Corresponding inverter does not exist." is displayed.
What are the possible causes?
The recommended connection cable MR-J3USBCBL3M is used.
Category : 

Answer

Check the version of FR-Configurator (FR-SW3-SETUP-WJ).
If the version is "1.00", it does not support or detect the FR-E740.
Version "2.00" supports the FR-E740. Upgrade the version from the Mitsubishi Electric FA Global Website.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700