• No : 21337
  • Release Date : 2018/08/22 16:27
  • Print

Parameter copy

How do I copy the parameter to the FR-E500 when replacing the FR-E500 with FR-E700?
Category : 

Answer

The copy function of the parameter unit (FR-PU04) is not available. Setting each parameter again or using the convert function of FR Configurator (FR-SW3-SETUP-WJ) setup software are the only way to copy the parameter.
Please consider to use the setup software.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700