• No : 21339
  • Release Date : 2018/08/22 16:27
  • Print

Input phase loss

An error "E.ILF" is displayed with the FR-E700.
Since it was an input phase loss error, I checked the power supply but the phase was not lost.
Are there any other possible causes?
Category : 

Answer

The FR-E700, D700, F700PJ may activate input phase loss protection "E.ILF" if the phase-to-phase voltage of the power supply has become largely unbalanced.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ