• No : 21378
  • Release Date : 2018/08/22 16:27
  • Print

Vector motor

What is the difference between the constant-torque motor, vector inverter motor, and servo motor?
Category : 

Answer

The constant-torque motor and vector motor are the induction motors, which consist of the stator core, gap, and rotor core.
For the constant-torque motor, the cooling ability at low speed operation has been improved, which enables the continuous operation with the constant-torque at the low-speed operation.
The vector motor is a dedicated motor for the vector inverter. The encoder is provided as standard, which enables the continuous operation with the constant-torque at the low-speed operation.
The rotor of the servo motor (synchronous type) consists of permanent magnets, and the stator consists of the coil to which current is applied.
Product Name
Inverter, magnet motor drive
Series
Others