- No : 21379
- Release Date : 2018/08/22 16:27
-
Print
Common connection of the terminal SD
When the 16 points common output type of the programmable controller is connected to the STF input of the multiple inverters, the terminal SD of each inverter is to be connected. Is there any problem with the operation?
- Category :
-
Answer
There is no problem for only the terminal SD connection because undesirable current will not be flown.
- Product Name
- Inverter, magnet motor drive
- Series
- Others