• No : 21380
  • Release Date : 2018/08/22 16:27
  • Print

Remote operation of the inverter

I want to perform remote operation of the inverter with the different enclosure contact. How long can I extend the control circuit and input signal (contact) circuit? (Example: 100 m etc.)Also, what is the voltage of this circuit?
Category : 

Answer

The wiring length of the start signal (STF etc.) is 30 m or less.
The circuit voltage of the control input signals (terminal STF etc.) is 24 VDC and the voltage when contacts are open is from 21 to 27 VDC.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500