• No : 21401
  • Release Date : 2018/08/22 16:27
  • Print

Surge voltage of 400 V inverter

It is explained that surge voltage is influenced by the switching speed of the inverter. Therefore, can motor burnout be prevented by lowering the carrier frequency?
Category : 

Answer

No. Although the carrier frequency increases or decreases the switching count, the switching speed is the OFF-to-ON speed of the IGBT element of the inverter.
Therefore, lowering the carrier frequency does not change the switching speed and cannot prevent motor burnout.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-S500, FR-A024, FR-E500, FR-A100, FR-F500, FR-A200, FR-A500, FR-V200