- No : 21433
- Release Date : 2018/08/22 16:27
-
Print
FR-A5CN03
I want to install the heat sink outside the enclosure using the FR-A5CN03, but the environment is bad and it is exposed to the spray of water there. Do I need some waterproof measure?
Let me know how to do it.
- Category :
-
Answer
Since the heat sink and fan are not waterproof, you need to enclose them so that they are not exposed to the spray of water.
If you use the inverter (heat sink and fan) in a closed environment, you need to take a measure to cool it.
Refer to "Enclosure Design" in Section 2.7 of the A500 and E500 technical material.
- Product Name
- Inverter, magnet motor drive
- Series
- Others