- No : 21464
- Release Date : 2018/08/22 16:27
-
Print
Connecting voltmeter to terminal AM
I am considering to connect two voltmeters (YM-8DV) to the terminal AM of the FR-A540-0.4K.
Can I connect them in parallel?
- Category :
-
Answer
You can connect them in parallel.
Connect the voltmeters in parallel, paying attention to the following:
- The output current should not exceed the permissible value of 1 mA when the output voltage of the terminal AM (maximum output) is 10 V.
- Product Name
- Inverter, magnet motor drive
- Series
- Others