• No : 21494
  • Release Date : 2018/08/22 16:27
  • Print

Auxiliary input power supply

Using two frequency setting potentiometers (1/2 W, 1 KΩ), I want to control the stall prevention operation level with the speed control terminal (terminal 2) and auxiliary input terminal (terminal 1).
Can I connect these two frequency setting potentiometers in parallel to the terminals 5 and 10?
If not, are the terminals 10 and 10E different power supplies due to their voltage difference?
Category : 

Answer

If you connect two frequency setting potentiometers to the terminals 5 and 10, the permissible current of 10 mA is exceeded, and you need to install 2 KΩ resistors. (You can connect two frequency setting potentiometers in parallel.)The terminals 10 and 10E are different power supplies.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500