• No : 21511
  • Release Date : 2018/08/22 16:28
  • Print

Inverter loss

Should I consider that the efficiency is exactly as mentioned in the material (for economy analysis)?
Category : 

Answer

The inverter efficiency changes depending on the inverter output frequency, carrier frequency, motor capacity, and load factor.
When the inverter and motor have the same capacity and are under 100% load, efficiency is 95%.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100