• No : 21522
  • Release Date : 2018/08/22 16:28
  • Print

Do you have a sample program for 485 communication?

I am planning to operate the FR-E500 from the programmable controller via RS485 communication.
Do you have a sample program to do this using the MELSEC-A or FX on the programmable controller?
Category : 

Answer

We do not offer a sample program for the programmable controller.
Refer to the Instruction Manual and create the program by yourself.
Product Name
Inverter, magnet motor drive
Product Category
Others
Series
FR-E500