• No : 21568
  • Release Date : 2018/08/22 16:28
  • Print

Amount of heat generated

How much heat does the vector inverter generate?
Category : 

Answer

The following amount of heat is generated under the 100% load. (The same amount for both the 200 V and 400 V classes.
The amount of heat generated by the built-in brake resistor is not included.)

<<Amount of heat generated by vector inverter>>
- 1.5K ????? 150 W
- 2.2K ????? 240 W
- 3.7K ????? 330 W
- 5.5K ????? 440 W
- 7.5K ????? 670 W
- 11K ????? 860 W
- 15K ????? 1100 W
- 18.5K ????? 1300 W
- 22K ????? 1750 W
- 30K ????? 2100 W
- 37K ????? 2400 W
- 45K ????? 2700 W
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200