• No : 21583
  • Release Date : 2018/08/22 16:28
  • Print

Can I input speed setting externally with the box type?

Can I input speed setting externally with the box type?
Category : 

Answer

No.
Use the potentiometer on the box to set the speed. If you want to input analog values externally to set the speed, use the unit (module) type.
Product Name
Inverter, magnet motor drive
Product Category
Inverter speed controller
Series
SC-A