• No : 21625
  • Release Date : 2018/08/22 16:28
  • Print

Communication option

Can I use the communication option FR-CU01 with the FR-A200 (E)?
Category : 

Answer

You can remove the parameter unit FR-PU02 and install the FR-CU01 there.
However, since the interface for the parameter unit is used, the communication speed is lower than the computer link plug-in option.

Similarly to the FR-PU02, the FR-CU01 can be installed and removed while the inverter is powered ON.
Product Name
Inverter, magnet motor drive
Product Category
Others
Series
FR-A200