- No : 21627
- Release Date : 2018/08/22 16:28
-
Print
Comparison of noise with FR-A200
Does the FR-A200EXCELLENT produce less noise than the FR-A200?
- Category :
-
Answer
The setting ranges of the carrier frequency are:
- FR-A200: 2 kHz to 14.5 kHz
- FR-A200EXCELLENT: 0.7 kHz to 14.5 kHz
The range of the FR-A200E is extended to the lower side, meaning that you can set the carrier frequency lower than the FR-A200.
This means that noise can be reduced than the FR-A200.
However, for the same carrier frequency, the noise levels are almost same.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200