• No : 21628
  • Release Date : 2018/08/22 16:28
  • Print

Compatibility of the function with FR-A100

Are the functions of the FR-A100EXCELLENT and FR-A100 compatible?
Category : 

Answer

Yes.
Compared with the FR-A100:- The PI control function is added.- Fast-response current limit operation is improved.- Cumulative energy monitor is added.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100