- No : 21633
- Release Date : 2018/08/22 16:28
-
Print
Maximum short-time torque
How much low-speed torque can be output under magnetic flux vector control?
- Category :
-
Answer
When the Mitsubishi standard cage-induction motor (SF-JR 4P) and inverter of the same capacity are combined, the maximum short-time torque under magnetic flux vector control based on 60 Hz torque is as follows:
150% torque for 1 Hz (0.4K to 55K), 200% torque for 3 Hz (0.4K to 3.7K). Refer to the figure below for details. Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200