- No : 21638
- Release Date : 2018/08/22 16:28
-
Print
What functions are added compared with FR-A200?
What functions are added to the FR-A200EXCELLENT compared with the FR-A200?
- Category :
-
Answer
The following functions are added or improved:
- Auto tuning function- Fast-response current limit operation is improved.- Characteristics of magnetic flux vector control is improved.- The carrier frequency setting range is extended.- Communication speed of plug-in option is improved.And others.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200