• No : 21640
  • Release Date : 2018/08/22 16:28
  • Print

Can I change the carrier frequency?

Can I change the carrier frequency?
Category : 

Answer

You can change it by changing the setting of Pr.72 (PWM frequency selection).
Setting range of Pr.72: 0, 1, 2, 3, 4, 5, 6 (Initial setting is "6".) (The smaller the value is, the lower the carrier frequency becomes.)

Be sure to change the carrier frequency while the inverter is stopped.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200